Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Do not edit the following entries! The entries are in the plinkcommon.cfg file under $CADENAS_SETUP.
Join statement defines, which primary key is assigned to which foreign key in the LINKTABLE and ERPTABLE. In this case „erp_pdm_number“.
PRJTABLE is used for the function Edit project table (see Section 5.21.7.7, “ Edit project table ”).
The TREETABLE is needed in order to display the red-green status in the directory tree. As of V9 this is necessary due to the new index structure (especially because of links).