Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This module enables the integration of company own META data into the PARTsolutions software.
With this, you can connect attributes from the META data, such as for example internal article numbers, prices, material, part status, etc, with the installed standard attributes of the PARTsolutions supplier catalogs.
The module contains the following functionalities:
PARTlinkManager ― Administrative tool for all ERP relevant data[73]
PARTadmin ― Configuration tool for PARTsolutions administrative tool for roles and users[74]
PARTsolutions Plug-Ins ― Enhancement for PARTsolutions, in order to integrate the ERP functionalities in all program parts.[75]
Database scripts ― Predefined scripts for creating the LinkDB, which can be used with PARTsolutions.[76]
Note | |
---|---|
|
The module is independent of the CAD interface used.
[73] Detailed information can be found under Section 5.7, “ Configure ERP environment ” and Section 5.8, “Data administration ”.
[74] Detailed information can be found under Section 5.6, “ User-Role concept ”.
[75] Detailed information can be found under Section 5.4, “PARTdataManager – ERP/PDM extensions ”.
[76] Detailed information can be found under Installations Skript.
[77] Detailed information can be found under Section 5.1.4.2, “ Data transfer and data link”.