Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
PARTcommunity can be hosted on one or several servers. The software requirements control the hardware requirements. Therefore only a recommendation for the hardware needed can be given.
We recommend splitting the software onto several servers:
(Recommendation: Setup of an own server for this software part. This requires a complex and very special installation incl. PARTsolutions client installation)
(Reuse of existing server possible)
Needed storage: Depends on the number of catalogs installed (PARTsolutions storage) + storage for preview images if special PARTcommunity images are desired.
Needed storage: Depends on the number of users/shopping cards (1 MByte * Number of Users)
A fast running and highly available network as well as low response times are required for all servers, of course.
Virtual servers are supported. The only exception with virtual hardware is the licensing: In that case a FLM server is required in addition. This FLM server must not be a virtual server[65].
If installing PARTcommunity at a physical machine, a regular nodelocked license can be used.