Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
PARTsolutions variables and all LinkDB fields (if an integration is available) [standard name "NB", bill of material name "LINA", etc.] can be transferred via attribute mapping in the list fields of the model attributes of ModelManager during export.
For the attribute mapping there are two different attributes:
The two attribute types are stated under "Attr_Custom_01[59]or 02. Compare example below.
Under Attr_Content_01 or 02 sections are stated, where the desired mapping parameters are listed.
If you want to use attribute mapping, then proceed as follows:
[AttributeMapping(is3d)] ;Attr_Content_01(is3dPart)=ModelManagerAttributesPart ;Attr_Content_01(is3dAsm)=ModelManagerAttributesAsm ;Attr_Custom_01(is3dPart)="PSOL_PART" :class-name "LIBRARY_3D" :attachment :contents :allowed-owner-types :part-assembly ;Attr_Custom_01(is3dAsm)="PSOL_ASM" :class-name "LIBRARY_3D" :attachment :contents :allowed-owner-types :part-assembly ;Attr_Section_01=MODELMANAGERATTR ;Attr_Content_02=MODELMANAGERATTRMASTER ;Attr_Custom_02="PSOL_MASTER" :class-name "MASTERDATA" :attachment :contents :allowed-owner-types :part-assembly ;Attr_Section_02=MODELMANAGERATTR [ModelManagerAttributesPart] NB=NB [ModelManagerAttributesAsm] LINA=LINA [MODELMANAGERATTRMASTER] NT=NT
The constants of the following list can be used as attribute values.