Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Basic settings, such as for example visibility or position of the icon, can be found in the [settings] block.
[settings] name=Table view of parameters icon=$CADENAS_SETUP/bitmaps/windowmode_table.png tablemode=table tablemodesignal=table menuvisible=1 toolbarVisible=1 Position=1
The following explains the individual keys:
name=Table view of parameters
The name is displayed in the window menu and in the short info of the icon.
In the "icon" key, the path to the icon to be displayed is given.
icon=$CADENAS_SETUP/bitmaps/windowmode_table.png
Chooses the corresponding tab page during the selection via the icon (Table or List).
tablemode=table
During selection, chooses the corresponding icon via the tab page (List view of parameters or Table view of parameters ). The List view with large 3D view icon is not connected to a tab page and does not contain this key.
tablemodesignal=table
menuvisible=0/1
toolbarVisible=0/1
With incrementing numeric value, gives the position in the toolbar from left to right, or in the menu from top to bottom.
Position=1/2/3/etc.