powered by CADENAS

Manual

Manual

2.2.7. Transfer attributes via CNS classification

If from the supplier's side the physical attributes have been set via CNS classification, these are transferred to the CAD system and are found in the respective "Physical properties" dialog. Within the physical properties the material has priority.

The data of the CNS classification is displayed in the Part information in PARTdataManager.

  • Physical properties

    • Mass

    • Volume

    • Density

    • Material

    • Volume and center of gravity

  • Object attributes

    • Order number

  • geometrical attributes

Detailed information is found in the PARTsolutions User manual under the topic "Physical properties from PARTsolutions" in the respective CAD specific sections.[56]



[56] Use the current CNS classification!