powered by CADENAS

Manual

Manual

4.16.3.1.1. Preparation
  1. Install Bikecompany V1.

    PARTadmin -> Catalog update -> Offline

    PARTadmin -> Catalog update -> Offline

  2. Import all projects of "Bikecompany" into PARTlinkManager.

  3. Assign ERP numbers to the single lines.[87]

    Mark all datasets and click on Assign ERP numbers in the context menu.

  4. The dialog box Generate value sequence opens.

    Click on Generate and then confirm with Ok.

    -> The automatically generated ERP numbers are assigned.

  5. Mark all datasets again and in the context menu, click on Set fields -> Active status.

  6. The dialog box Set values opens.

    In the list field select Released and confirm with OK.

  7. Now the PARTlinkManager shows a small, but realistic initial situation. With the help of this data the functions of the Update manager are explained.

    Initial situation: 3 projects with 9 datasets altogether

    Initial situation: 3 projects with 9 datasets altogether

  8. Open PARTdataManager and select the catalog "Bikecompany".

    PARTdataManager catalog "Bikecompany" V1

    PARTdataManager catalog "Bikecompany" V1

  9. Open the projects "Piston", "Piston ring" and "Spoke".

    Project "Piston"

    Project "Piston"

    Project "Piston ring"

    Project "Piston ring"

    Project "Spoke"

    Project "Spoke"

    The status light is on green at all projects.

In the next section a catalog update is conducted.



[87] You can do this in PARTdataManager via Add dataset to link database or how it is explained here in PARTlinkManager.