Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.2.4. FLM
Server Installation - Request/install licenses
2.2.4.3. Installing FLM server (Master)
|
|
---|---|
Prev | Next |
After having installed PARTsolutions you must get licenses for the clients/terminals from a central FLM server.
a separate computer[12] (at client/server and also for single workstations)
From this
computer open the start screen (start.exe
) and choose
Installation (License
server).
Follow the directions of the installation routine. In the window Choose Destination Location a path has already been suggested, however you may change it if you like.
--> The copying process of data starts.
After completed installation of the FLM server, please check if the required service runs properly.
In the WINDOWS start menu, please open the directory Settings/System control/Administration/Services.
--> You should then find the service CNSMASTERSERVER V9 . In its row you should see status "Started" and in the field Autostart "Automatic" should be set.
If these settings are not available, double click on the respective field and adjust the settings in the window which opens.
[12] The FLM server can also be one of the clients. As such it must be available in the network at all times of course.