powered by CADENAS

Manual

Manual

10.5.4.3.7. Delete

Delete Element :

  1. Click on the element that you want to delete in the 2D drawing.

  2. Select Delete Element.

The order in which you carry out steps a) and b) is irrelevant.

--> In the 2D drawing, the element is removed, however in the History the according Feature remains intact. A relation line from the feature Delete Element to the feature of the deleted element (see figure.) occurs. This relation line can only be seen by you when you let the secondary features be displayed.

 
  1. You may undo the deletion process.

  2. To do so, right-click on the context menu of the Delete Element feature.

Select Delete step.

Delete element with condition :

Assign a Condition to the Delete function.

  1. Follow the same steps as with the Delete Element function (above).

--> The Change parameter window opens.

  1. Enter your desired Condition and confirm with OK.

--> In the example, the marked line will only then be created if the value for variable H is greater than 8.

[Note] Note

Provisional deletion should only be used with individual sketch elements. Do not connect the entire sketch to a condition since this can then become completely invalid.

It is highly recommended to create a corresponding Condition in such cases via the context menu of the respective Features (history) (see example below).).