powered by CADENAS

Manual

Manual

10.7.5.1. Case 1 - Export 3-D part to 3-D CAD system

  1. Click on the Export in file menu icon. -> A selection of different 3-D export and graphic file formats [a] (BMP, JPEG, TIFF) shows up (see figure).

  2. Per mouse-click, select the format that fits your CAD system the best from the available export formats,for example, the AutoCAD file format DXF 3D.

Export in file

Export in file

[a] The selection of export formats depends on the respective license.

[Note] Note

The symbol (icon) for the file format overviewchanges. It keeps the lastly selected symbol until a new export format has been selected.

  1. A window in which you can assign the storage location (Filename field) and version status (Version field) of the file shows up. The Documents folder in the User directory is preset. Using the Browse ... button, you can open the Explorer window Save as.... Enter a file name an click on the button Save. The close the window with OK.

    Export in xy format

    Export in xy format

[Note] Note

Please make sure that the file expansion (for ex. *.dxf ) is included.

  1. Open the file from your CAD system. The example shows the storage location that has been assigned via the Windows Explorer.