Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Show graphics in table (if available) : A table may also contain columns with graphics. If you wish to also display these files per default, please check this option button. Hereby only the preselection is controlled. Via Default toolbar -> Show graphics in table you can switch on and off the graphics anytime.
Show only preferred rows : Restriction of the table on preferred rows (see fig. below).
If you like to switch on the preferred rows as default, then check the option. Hereby only the preselection is controlled. Via Default toolbar -> Preferred rows on/off you can switch on and off the restriction of the table on preferred rows anytime.
Variable for preferred rows :In this field you can set the variable and/or column, that should be pulled up as the preferred row. The column appointed here has precedence compared to the setting in the project.
When the function is switched on, then in the table only these rows are displayed which have an entry in the set column.
Variable for alternative part : If you set a checkmark here the part, which is closest to the preferred part in the table, will be transferred to the CAD system as a meta file. This function is only supported by certain CAD systems.
With activated option the class variables are displayed in addition according to the selected classification (here exemplified eClass 5.0). This functionality is also available for your own classification. Section 5.7, “Apply own Class system ”.
When you wish to differentiate identical parts via the material then activate the Show material selection option.
Thereby in the table a "virtual" column "CNSMAT" is displayed for the material selection.
Before the export you open the Enter value dialog with a click into the respective field.
In the
Enter value dialog all materials are listed
which are set up in the material.cfg
.[65]
Table restrictions : Via conditions you can restrict the table. For example D > 20. The combination of conditions is possible as well: D>20.AND.K>15.
Columns to hide : Columns not to be displayed can be specified here. For several columns use comma separation.
Font for table : Choose from the available types via Browse .
The font size is adjusted consistently for the table view and list view.[66]
[65] Administrative notes on this you can find under Section 2.2.5.1, “Material mapping without ERP integration ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
[66] As of V9.05 the font size is adjustable for the list view.