Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
The information in fields DIN / ISO-IDand Unitis optional. Neither is it absolutely necessary to define a unit if data type "Number" is set. |
Description : A description text may be added to the variables. If you click in PARTdataManager on the variable name later, this description is then displayed. |
Due to the meaning of the type of identification you can find commentary at the end of the list in its own paragraph.
See also Section 1.1.6.7.20.3.2, “ Key "LockDimRange" ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
Within the system, the difference based on the Status is also relevant.
The data is located in the corresponding *.tab file. Table values can be edited directly in the PARTeditor GUI. With this setting, a check mark is automatically set for Display, Set. |
|
The value of a variable can be calculated by a so-called attribute algorithm. Dependences/conditions between variables can expressed with attribute algorithms. Example 1: "If D1=12, then D2=D3". In this case, an attribute algorithm must be stated for var i able D2. Example 2: if a variable has a constant value, e.g. "D2=20", an algorithm can also be used. Please refer to Section 8.5.2.7, “ Attribute algorithms ” if you define attribute algorithms. |
|
Variables whose values lie within a defined range, e.g. "10 to 20" or on which several fixed values are available for selection are assigned status Value range variables. Please refer to Section 8.5.2.6, “ Value ranges ” for how to define value ranges. |