Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The difference of characteristics to characteristic types is of special importance for the ERP/PDM integration!
Values that are necessary for dimension and/or product standards.
For order numbers or technical specifications, etc. (Characteristics that do not have anything to do with geometry or function)
Note | |
---|---|
Using the example of a cylinder, the distinction between the stroke, which is a Geometry attribute and the rod positioning, which is a Function attribute. By activating the ERP functionality the stroke is pinned, as soon as an ERP_PDM_NUMBER has been attributed (the rod positioning does not get pinned). The pinned state becomes visible through the columns with the white background (see table below). Strokes are also assigned different identification numbers in the ERP functionality; different rod positioning is not. See Section 1.1.6.7.20.3.2, “ Key "LockDimRange" ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |
Between geometry and object attributes there is no functional difference, they are currently being dealt with equally.
Dimension attributes are used with half-finished products and profiles that do not have fixed dimensions. The length (L) can be cleared within the default value range before export. |
With the customizing of PARTsolutions, in accordance with ERP guidelines, it is decided whether a part with different lengths obtains different identification numbers, or if the identification number remains the same. In the first case, the corresponding field will be pinned (white background), in the later, not.