Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Restricted Display : define the Conditions (e.g. DG=8[25]) for reducing the table display to specific values (see illustration below).
Suppressed Rows :Similar to the restrictions by preferred rows, the table display can be reduced here. This restriction however - in contrast to the preferred rows function - cannot be turned on/off, it is fixed.
If you wish to reduce the number of table rows shown using filters in a project, first define one or more filter variables [a]in PARTeditor. Now enter the required filter in the individual rows of the filter variable. In the PARTdataManager [b], in the Extras menu, Settings, Part selection dialog page, in the Project filter field you can control the number of displayed roles via the filter. |
|
[a] Filter variables must be of type "text". They are created in addition to the existing variables. [b] As of version 8. |
[25] In this context the more complex syntax is possible as well. Please read Section 8.5.2.7, “ Attribute algorithms ”.