powered by CADENAS

Manual

Manual

4.8.2.4.3.  Variables containing external references

Columns can be provided with the feature to start a program or to open a document when clicking into the column. Define the respective column under PARTproject -> General1 -> Variables -> Variables containing external references. After this it is highlighted in green.

  • Document to open:

    Define the document which shall be opened when clicking on the defined column.

    The document (also several for different languages) has to be stored in the project directory.

    If documents are available in several languages attach a language ID to the file name separated by an underscore. In the example below "_english" and "_german".

    In PARTproject -> General1 -> Variables -> Variables containing external references -> Document to open set the following entry:

    info_$CADENAS_LANGUAGE..txt[24]
    

    Explorer - Additional documents

    Explorer - Additional documents

    PARTproject - Document to be opened

    PARTproject - Document to be opened

  • Executable (WIN):

    Define the program (*.exe) to be opened when clicking on the defined column (WIN)

  • Program to be carried out (UNIX):

    Define the program (*.exe) to be opened when clicking on the defined column (UNIX).



[24] The two points one after another are correct: The first point belongs to the variable declaration.