Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The tabbed page Catalog help always shows up at directory level.
--> The dialog page Catalog help opens.
On this dialog page you can set buttons, help texts and documents and deposit them as defaults. The actual allocation to directories and projects occurs on the register page itself. Close this page with after you have completed all entries.
In the field Catalogs set the directory that should acquire the new help. For example, "demo_catalog". You create new lines via the button.
Enter the bitmap symbol for your Help file in the Catalog buttons field.
If the corresponding file lies outside of the PARTsolutions installation path, you will see a prompt as to whether you wish to copy it beforehand to the directory of the catalog you specified beforehand. Confirm with Yes .
Under Help strings (these show up as tooltips) set the optional default text.
You are now once again on the dialog page Catalog help.
At the left of the directory tree, choose the directories and projects in order to create the desired settings in dialog area specifically.
In the Help strings field, tool tip texts [26]can be applied in different languages. Set "German" and enter your help text. This text will later be shown upon passing over with the mouse arrow in the PARTdataManager.
You can save Help documents in various languages in the Documents field. Also set "English" and enter the path to the document file which is to be opened when you click on the button in PARTdataManager.
Tip | |
---|---|
Use $CADENAS_DATA/help/demo_catalog/... The directory has already been set during the creation of the button symbol. |
[26] Tool tip: Short explanatory text which shows up upon touching with an interface element, for ex., a button.