powered by CADENAS

Manual

Manual

6.10.2.1.5. Installation of catalog update (at the customer)

[Tip] Tip

Under Catalog update -> Online, in a first step only download the CIP file.

Therefore uncheck Install after download.

Then switch to the variant Catalog update -> Offline. When using the offline variant you can check the ERP status (possibly PLM status in addition) of datasets BEFORE the installation. Furthermore the functions Check and Compare are available.

In the following the procedure of an offline catalog update is explained.

  1. If under Catalog update -> Online, you deactivated the option Install after download, then the downloaded catalog cip files can now be found in the temporary Download directory, which you determined in the settings dialog.

    Open the CIP file by clicking on Open (selection in an Explorer window).

  2. Click Install.

    -> The dialog box CIP Installation with the options Yes - Check Catalog and No - Install now opens:

    • Yes - Check Catalog

      It is checked whether there are datasets with status to check and/or not mapped.

      [Note] Note
      • to check: Actually this status should not occur, because publishing without ERP mapping is not allowed.

      • not mapped: This status shows up with faulty mapping or installation or missing mapping.

      • If datasets with status to check or not mapped are found during a test run, in the dialog box CIP Installation the tabs Protocol, ERP Status and PLM Status are displayed, otherwise the installation is immediately performed.

        [Note] Note

        If you want to make a check in any case, do not click on Install but on Check (see below).

        • Protocol tab

          On the tabbed page Protocol the number of datasets per Status is listed (details further below): (Same result as with Simulate ERP update, compare Fig. „Tabbed page Protocol “).

          • successful (incl. checked)

          • expired

          • to check

          • not mapped

          Dialog box "CIP Installation" -> tabbed page "Protocol"

          Dialog box "CIP Installation" -> tabbed page "Protocol"

        • ERP Status tab

          For all affected ERP numbers the status (checked, successful, expired and not mapped) is displayed, furthermore Path, Path (new), NB and NB (new).

          • checked: Mapping verified by mapping file (green checkmark)

          • successful: The automatic check was successful, identifying projects which do not need to be verified. They can definitely occur in the mapping dialog. And they are all the ones without icon occurring because the tab file changed but without need for mapping (e.g. new row added).

          • to check: Actually this status should not occur, because publishing without ERP mapping is not allowed.

          • expired: Rows verified with a red x , meaning rows, which do not exist anymore, furthermore rows which have been mapped to "nothing" by Conditions.

          • not mapped: This status appears at faulty mapping, error during installation or missing mapping.

          Dialog box "CIP Installation" -> tabbed page "ERP Status"

          Dialog box "CIP Installation" -> tabbed page "ERP Status"

          If in the dialog box CIP Installation, the tabs Protocol, ERP Status and PLM Status are displayed, then there are datasets with status to check [68]and/or not mapped.

          That means editing via Update manager [69] is needed.

          [Note] Note

          Status not mapped has to be confirmed in the Update manager.

          If after the check the installation shall be performed, at desired catalogs, activate the checkbox and click on Install selected catalogs otherwise on Cancel.

          [Note] Note

          If problems occurred, at the end of the installation following note is displayed:

          There were mapping problems in the LinkDB. Please correct these in the UpdateManager.

          When clicking on the link you are redirected to the Update manager.

        • PLM Status tab

      • If there are no datasets with the note to check or not mapped the installations runs through without further note. Then, at the end of installation the tabs Protocol, Status and ERP Status are displayed again - this time in the standard dialog area under Catalog update -> Offline.

    • No - Install now

      The installation is immediately started. At the end of the installation the tabs Protocol, Status and ERP Status are displayed - this time in the standard dialog area under Catalog update -> Offline.

Result after processed installation:

At the end of the installation the tabs Protocol, Status and ERP Status are displayed - this time in the standard dialog area under Catalog update -> Offline.

  • Protocol

    The tabbed page Protocol is opened by default.

    If problems occurred, on the tabbed page Protocol, the note There were mapping problems in the LinkDB. Please correct these in the UpdateManager. is displayed.[70] At the first catalog update with V10 or V11 the mappings still have to be manually created for a last time (with them Update manager), but after this the new method is effective and manual editing is only needed in seldom exceptional cases if an automatic update is not possible.

  • Status

    On the tabbed page Status, you can find a detailed listing of the individual projects.

    The following table shows the meaning of symbols (icons)

    Field/Column

    Meaning

    P

    ...stands for project

    T

    ...stands for table

    3

    ...stands for 3D view

    !

    First publishing

    >

    New version

    =

    Same version

    x

    deleted

  • ERP Status

    On the tabbed page ERP Status you can find a listing of all ERP numbers with its update status (successful, expired, to check and not mapped), a furthermore old path, new path, old NB and new NB. Explanations on the individual status can be found above.

Update manager

By default, on the tabbed page Protocol, the note There were mapping problems in the LinkDB. Please correct these in the UpdateManager. is displayed. When clicking on the link UpdateManager it is opened.

You can simply check whether there is something to edit: In the Update manager, deactivate the button Show mapped lines .

-> Then on the right under Line mapping, only those rows are displayed where there were changes which are not confirmed yet.

If everything could automatically be assigned, then nothing is selectable anymore. Otherwise perform the mappings with the help of the Update Manager. Details on this can be found under Section 4.16.3, “ Catalog update with ERP integration - Fix mapping problems with the Update manager ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

Button "Show mapped lines" is activated.

Button "Show mapped lines" is activated.

Button "Show mapped lines" deactivated: Only folders with icon are displayed (here in this example none).

Button "Show mapped lines" deactivated: Only folders with icon Button "Show mapped lines" deactivated: Only folders with icon are displayed (here in this example none). are displayed (here in this example none).

PARTlinkManager

If you are using the variables ACTIVE_STATE and/or REQUESTED_STATE in the ERP set of rules, have a look on the status in the PARTlinkManager.

You will have better overview when activating the button Hide old versions of parts .

At all hidden or filtered projects ACTIVE_STATE has been automatically set on Released.

If needed you can manually set the status under Set fields.

Simulate ERP update

Further you have the possibility to fetch information on changes before the catalog update (even if only the status successful and/or expired occurred, meaning no editing in the Update manager is necessary.

  1. Click on Check.

    -> The dialog box Check opens.

  2. Click on Simulate ERP update.

    -> A test run is processed.

  3. Again, in the dialog box the tabs Protocol, Status and ERP Status are displayed.

    • Protocol

      On the tabbed page Protocol an overview is shown, subdivided by the following categories:

      • Records successful

      • Records expired

      • Records to check

      • Records not mapped

      Tabbed page Protocol

      Tabbed page Protocol

      • Export status: A respective dialog is displayed.

        Choose the desired option and click on Export.

        • Export all

        • Export deleted (x)

        • Export new (!)

        • Export updates (>)

        -> An Explorer window is opened.

        Determine the location for a CSV file and confirm with Save.

      • Export ERP Status

        -> An Explorer window is opened.

        Determine the location for a CSV file and confirm with Save.

    • Status

      On the tabbed page Status, you can find an exact listing of the single project's status.

      The following table shows the meaning of the symbols.

      Field/Meaning

      Meaning

      P

      ...stands for project

      T

      ...stands for table

      3

      ...stands for 3D view

      !

      First publishing

      >

      New version

      =

      Same version

      x

      Deleted

    • ERP Status

      On the tabbed page ERP Status you can find a listing of all ERP numbers with their update status (not mapped, checked, successful and expired), furthermore Path, Path (new), NB and NB (new). Explanations on the individual status can be found above.



[68] Actually the status to check should not occur if an ERP mapping has been performed, which is mandatory for publishing.

[69] Detailed information on Update manager can be found under Section 4.16.3, “ Catalog update with ERP integration - Fix mapping problems with the Update manager ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

[70] On the tabbed page Status ERP you can see for which. This are the ones marked as to check or not found.