The ARC fusion reactor (short for affordable, robust, compact) is a theoretical design for a compact fusion reactor developed by the Massachusetts Institute of Technology (MIT) Plasma Science and Fusion Center (PSFC). The ARC design aims to achieve an engineering breakeven of three (to produce three times the electricity required to operate the machine) while being about half the diameter of the ITER reactor and cheaper to build.The ARC has a conventional advanced tokamak layout, as opposed to other small designs like the spherical tokamak.
The ARC design improves on other tokamaks through the use of rare-earth barium copper oxide (REBCO) high-temperature superconductor magnets in place of copper wiring or conventional low-temperature superconductors. These magnets can be run at much higher field strengths, 23 T, roughly doubling the magnetic force on the fuel. The confinement time for a particle in plasma varies with the square of the size and the fourth power of the magnetic field, so doubling the field offers the performance of a machine 4 times larger. The smaller size reduces construction costs, although this is offset to some degree by the expense of the REBCO magnets.
The use of REBCO also raises the possibility of allowing the magnet windings to be flexible when the machine is not operational. This offers the significant advantage that they can be "folded open" to allow access to the interior of the machine. Accomplishing this would greatly lower the cost of maintenance, which with other designs generally requires the maintenance to be carried out through small access ports using remote manipulators. If realized, this could improve the reactor's capacity factor, an important metric in power generation costs.
There is a plan to build a scaled-down demonstration version of the reactor, named SPARC, by the company Commonwealth Fusion Systems, with backing from Eni.