Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
To share its 3D models with friends or colleagues, users can use the PARTcloud.net 3D Printing & Sharing Community app. Models can be uploaded via PARTcloud.net on the 3D CAD models download portal PARTcommunity in STL and STEP format.
1. Users have to login at PARTcloud.net or create an account free of charge in order to enjoy all the advantages of the Sharing Community. If you are already registered for the 3D CAD models download portal PARTcommunity, this is also valid for PARTcloud.net .
The components are uploaded and the information as well as details filled in so that the 3D CAD model can be found more easily by other users.
2. After uploading, the 3D CAD model appears in your own portfolio.
3. Now the app PARTcloud.net 3D Printing & Sharing Community by CADENAS has to be installed on the smartphone or tablet.
4. In the app itself, the search field is used to enter searched terms - in addition, the two filter functions "newest" and "select a category" can be used.
5. Once you have found the 3D model, you have a well-known features, such as downloading the model. In addition, app users have the opportunity to link model and camera function to each other. Thus, two realities can be linked for spectacular photo shots.
1. Download the APP
2. Activate the SKETCHER
3. use the SKETCHER
The 3D radial menu is available in the web apllications PARTcloud.net, BIMcatalogs.net and the 3D CAD model download portal PARTcommunity app as well as the PARTcommunity web app.
A single tap - manifold selection
With only a single tap, different alignments of the 3D CAD models are displayed to the user and the model can be viewed from all angles. There is also the option of animated CAD models.
a. Front view (Z)
b. Rear view (-Z)
c. Left view (-X)
d. Right view (X)
e. Top view (Y)
f. Bottom view (-Y)
g. Isometric view
h. Animation
Moreover, various shading possibilities can be selected: The edges can be displayed or a combination of both possibilities is shown in a model.
a. Edges
b. Shaded
c. Shaded with edges
The 3D CAD model can also be used for different virtual realities and have them displayed.
a. Virtual Reality (Cardboard etc.)
b. Anaglyph view
c. Dreamoc HD3
d. Dreamoc XL2
e. Camera background
Additional features, such as dimensioning or screenshots, are also available to the user.
a. Scale to window size
b. Cut
c. Dimensioning
d. Explosion
e. Full screen
f. Leap Motion
In our video, you can see how the 3D radial menu looks on a mobile device:
Upload your 3D CAD models for free on PARTcloud.net and show them to your friends and co-workers with the PARTcloud.net app - IT IS FREE and FOR YOU !