For major projects (> 50000 parts) better generate preview images and indexes subsequently with PARTproject or PARTadmin.
Turn off generation of preview images
If dialog box PLM Synchro Wizard is not opened currently, call it under Processes.
Select the desired process and click on the context menu command Edit PLM Synchro process.
-> The Wizard is opened.
In the Export menu, deactivate the option Generate preview.
Generate preview images subsequently in PARTproject via context menu command Output -> Generate image data/preview images.
In the pipeline, select the node PARTsolutions Exporter.
In the Node Editor, under Indexing, select the option Custom.[8]
Under Indexing Settings, click on .
-> The settings dialog is opened. Select all items except Skip View Index.
Create desired indexes in PARTadmin under Index administration and respective context menu command on your created catalog.
If the "Any"
search shall be used (finding of topological dimensions of length via
Full-text search), then please regard to activate one of the keys
TopologyCatalogs
or
TopologyCatalogsRegex
in the
configuration file partsol.cfg
.
Details on this can be found under Section 1.3.8.6.2.2, “ Update Full-text search index (and Geometrical search index) for finding topological values via Full-text search ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
Use the Report node in order to log errors. See Section 1.2.2.9.1, “ Report node ”.
Use XML reader and XML writer in order to log failed parts and add to the process again. See Section 1.2.2.9.2, “ XML writer – XML reader ”.
Detect attribute names. See Section 1.2.2.9.3, “How to get attribute name”.
PARTsolutions Exporter -> Commit settings. See Section 1.2.2.9.4, “ PARTsolutions Exporter ”.