Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In order to edit classification attributes, do the following:
You now have the following options:
Delete new added attribute
again
Click into the
row to delete (concerning New mode[15]) and then on .
Confirm with . -> The delete command is processed and the dialog closes.
The columns of the Edit class window:
In the selection list you can carry out the following settings.
The Feature name field is only editable when New mode is used, thus for a new added row.
You can carry out the following changes in the selection list.
With lists of values or value ranges choose YES in the drop-down menu, otherwise No.
Description is available for every language.
Corresponding columns are set up for every applied language.