In
Details mode
(default) the variables of ALL results are displayed, which possibly
results in a wide table (if many catalogs have been searched or the search
provides different parts). So possibly fields remain empty, if the
respective part does not contain certain variables.[64]
Variable filters in the column header
At the top of each column you can see an input field for filtering. Even if not all hits are displayed in the search results, the filter affects all hits and the display of table variables is dynamically adjusted. You can filter a number of variables one by another, already entered values remain.
In the following example a search for "head cap bolt" and the numerical value "50" has been performed. Search terms are marked with yellow color.
You can position interesting variables further forward by drag & drop with pressed mouse button in order to view them at a glance.
In the following example nominal thread diameter, length and pitch have been filtered.
If there is not enough space to show all available information, this is signalized by the display of "more...". Especially, this could be the case in the columns Summary and Topology.
When searching for "schraube" in an English user interface, in the expanded view, you can see where the hit occurred.
Searching for topological values by Full-text search, may possibly deliver a lot of values. In order to see all values, click on "more...".
[64] you can change the display that only the variables of the respective result are displayed. On this see Section 3.1.6.7.2, “Columns show/hide ” -> Option "All table variables".