Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Via this dialog you can edit data from the ERPTABLE and some data from the LINKTABLE (Active status, Requested status.[83].
To change one or all fields of a dataset, click on the Edit button in the PARTlinkManager.
![]() |
Note |
---|---|
If more than one dataset has the same ERP number, these datasets are all equally affected by changes (edits). |
Load the part again; only then do the changes become visible.
[83] If you want to edit the geometries and/or create a variant, use the command Add dataset to link database (variant) (see Section 4.13.3, “Create variants in PARTdataManager ”) in the ERP toolbar of PARTdataManager or the context menu command Edit variant / Create variant in the PARTlinkManager (see Section 4.25.7.3, “ Edit variant ” / Section 4.25.7.4, “ Create variant ”).
Access to all data in the LINKTABLE and ERPTABLE can be reached with the extended function PARTdataManager -> ERP toolbar -> Edit/delete dataset (see ERP Symbolleiste).
Information about switching on the additional information can be found under Section 4.21.1, “ Load additional scripts - erpcustom.cfg -> Block [LOAD]”.