![]() |
4.24.5. "Roles" dialog
- Tabbed pages
4.24.5.6. Tabbed pages
Standard name , Standard name
(short) , BOM name
|
|
---|---|
Prev | Next |
![]() |
Important |
---|---|
The file name for the exported CAD document must be absolutely unique. The whole CAD
administration including the specification of the name rule is performed
via the CAD configuration file under Detailed information on the CAD administration in general is found under Chapter 2, PARTsolutions - CAD Integration - Administration. Detailed information on the creation of the file name in particular is found under Section 2.2.2, “Set file name ("FileName" key) and pool path ("poolpath" key) ”. By default, on
the tabbed pages Standard name,
Standard name (short) and BOM name, NO entries are performed! Then in
PARTdataManager, in
the 3D view, the standard NB and in the table docking window the
standard LINA is displayed and the setting under If entries are
performed on the tabbed pages Standard name,
Standard name (short) and BOM name then these will change the NB! This
again affects the setting under |
You can find the setting options both in PARTlinkManager and in PARTadmin. The syntax is identical.
If standard configuration options should not suffice, there are further extra options available::
Change NB according to project
If the NB is part of the naming rule the NB can be adjusted according to projects. In any case the basic rule is entered in the dialog area of the respective tabbed page.
See Section 4.25.7.7.1, “Change standard descriptions according to project ”.
If the options in the entry field do not suffice, you can generate a reference to a vbs script and work with complex conditions.
The call of the external script happens with NB=TSCRIPT('nb.ruletable','$CALCED_ROW.','$NB.').
Also see Section 6.1.6.1, “Example 1”.