![]() |
1.7.9.2.
Tweak
menus, menu items, toolbars, buttons and context menu commands
1.7.9.2.1. Overview
|
|
---|---|
Prev | Next |
All settings are handled with standard configuration files which are displayed in PARTadmin -> Category Configuration files -> $CADENAS_Setup.
Which application is controlled by which file can be seen directly at the file name.
menustructure_<name of application>.cfg
menustructure_PARTdataManager.cfg menustructure_PARTProject.cfg
"menustructure" configuration files define the basically structure, meaning which menus, menu items, toolbars, buttons and context menus are basically available.
Details on
menustructure_<name of
application>.cfg
can be found under Section 1.7.9.2.2.1, “menustructure_PARTdataManager.cfg”.
menuvisibility<name of application>.cfg
menuvisibility_PARTdataManager.cfg menuvisibility_PARTProject.cfg
"menuvisibility" configuration files define the visibility of UI elements.
The config is subdivided in blocks which represent certain modes Beginner, Professional or role-dependent modes [with ERP integration]).
Each mode contains a list of keys representing single functions/UI-elements (represented in menus, toolbars or context menus).
Key value can be true (element visible) or false (element hidden). Simply set the key value as desired. When clicking through the keys, on the right side, in the dialog area Documentation, the respective figures of the user interface are shown so that you can immediately see the relation between function element and config setting.
Details on this can be found under Section 1.7.9.2.2.2, “menuvisibility_PARTdataManager.cfg”.
![]() |
Tip |
---|---|
Also read the general notes under User interface at a glance and Full-text search. |