![]() |
1.7.9.2.
Tweak
menus, menu items, toolbars, buttons and context menu commands
1.7.9.2.4.
Settings in partsolu.cfg
|
|
---|---|
Prev | Next |
With the help of the key sortToolbars under $CADENAS_DEFAULT_USER -> block [TWEAKMENU] the position of the toolbars is saved. When restarting the application the set positions are recovered.
toolbarOrderTop=Standard,Assembly,Details,Export,\n,Views,LinkDatabase,Addsap,IndexTree
The value of the config key will be set to 0 when the application is closed.
Key PARTdataManager_Mode (or PARTproject_Mode)
The key saves the mode Beginner / Professional which is used when opening the application. Under Extras menu -> Select mode you can switch anytime.
Add further applications to be controlled by tweak configs
If you want
to add a new application, which should be controlled by the tweak
settings you must insert the name of the application as value of the
key processedApps in the $CADENAS_USER/partsolu.cfg
.
Create the two configs described above. Copy the content of menustructure_PARTdataManager.cfg
and menuvisibility_PARTdataManager.cfg
to get a quick start.