![]() |
Reset Resets the search fields and last sorting. | |
Via the entry field in the header of the table you can restrict the number of datasets . In the example the value of the price "0.10" is entered. --> According to the Query the table shows rows in which the field contents in the column "price" correspond to this default. |
|
Add row: Only applies a number. By the
following procedure this number will be linked to a dataset.
See also Section 4.13.1, “Creation of ERP numbers”. Double-click the line and thus call PARTdataManager. Select a certain variant/dataset. Click on the button Send selection to Link Manager
-> The dataset selected in the PARTdataManager is now connected with the assigned ERP_PDM_NUMBER. The view will switch back to PARTlinkManager without any linkage. |