![]() |
4.12.1. Create
users
4.12.1.4.
Create database user on the side of PARTsolutions via
PARTadmin (dialog "Database user")
|
|
---|---|
Prev | Next |
Database users
are saved in the configuration file plinkusers.cfg
.
In order to locally add users in PARTsolutions, do the following:
In the list field, select the used database type. (Here in the following figure exemplarily MS-SQL)
The login window Database login… appears.
In the list field under Database, select the desired database, to which you want to connect.
Log in with administrative rights, otherwise you cannot perform changes.
After successful login the button Load is active. After a click on the button all already created database users are displayed.
Dialog area Database user -> button Create locally
Using this
command means that the user displayed in the Database user window is collected in
PARTsolutions. The corresponding user then shows up in the User window. He is also taken over into the
plinkusers.cfg
configuration file.
[erpuser]
GROUPS=
GROUPORDER="DUMMY","LOC1","LOC2","LOC3","LOCRED1","LOCRED2",...
There are two Delete buttons. Please regard the difference!
Also see Section 4.12.1.3, “Create users on the side of PARTsolutions via PARTadmin (dialog User-Role assignment) / plinkusers.cfg -> Block <user name>”.