Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
1.3.9. PARTapplicationServer
installation/configuration
1.3.9.4. Connection of
external departments (HomeOffice)
|
|
---|---|
Prev | Next |
If a PARTsolutions client which normally is inside the central network, is started via Internet connection in external departments (HomeOffice), loading of required data possibly takes several minutes, which is due to the fact that it's about 1GB data (configuration files, scripts, etc.).
Increased performance in external departments (HomeOffice) can be achieved by storing $CADENAS (software) and $CADENAS_SETUP (configuration files, scripts, etc.) locally. $CADENAS_SITESETUP (it includes the modified files of $CADENAS_SETUP) may remain on the server and can be synchronized (client and server should have the same time) via the Site-Setup-Sync function (see Section 1.3.9.9.3.6, “ Site-Setup-Sync ”) or alternatively e.g. with the help of an external program such as Robocopy.