![]() |
Note |
---|---|
Make use of catalog updates. In this way best part quality is ensured. Via PARTupdate you can be notified on updates. On this see Section 4.5.2, “ PARTupdate - Notification on available catalog updates ”. |
During the initial installation the dialog for the selection of Standard part catalogs appeared in the installation routine.
You could select from the following Standard catalogs:
In order to post-install missing catalogs or to update already available catalogs (Standard catalogs or Supplier catalogs) use the online installation via PARTadmin.
You can call PARTadmin -> Catalog update -> Online directly from PARTdataManager.
When clicking on the button PARTadmin opens.
At the desired catalogs, activate the checkbox and click on Download/install selected catalogs.
![]() |
Important |
---|---|
It is expressly recommended, in the dialog area 3. Versions, either to choose the option Keep all or the option Number of versions >=2 (default 2). |
Details on catalog updates can be found under Section 1.3.3.1, “ Catalog update Online ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
For catalog new installations, of course you can install from DVD, too. On this see Section 3.1.2.1, “3D catalog selection: Standard and supplier part catalogs ”. Possibly the DVD catalog status is not up-to-date, so that actually the online update is the preferred option.
With existing ERP integration please regard the notes under Section 4.5.3, “Catalog update with ERP integration” in addition.
Notes on the relation between software and catalog status (Geometrical search index) can be found under Section 1.3.4.5.2.1.1, “Dependencies between software update and update of Geometrical search index ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.