![]() |
When a new
release CIP is generated via PARTproject, also a scanner is
running during this process in order to identify and classify all kind of
standardized parts. Explicitly all NNs and NTs are checked whether they
contain one of the below listed keywords followed by a number like “123”,
etc.: If this is the case, the project is automatically
assigned in
the Standards
classification of found Standard project's class. Projects of
this sort are marked with the Standards icon in PARTdataManager.
DIN, ISO, ANSI B, NF E, VDI, UNI, NAS, NASM, BSI, ASNA, JIS, CSN, STN, GOST, JB/T, NIHS
EN, SN, LN, AN, SN, BS, IS, KS, GB, PN, GB, MS, VG
Especially within the 2-digit keywords there is unfortunately a high rate of mistakes and wrong classifications, because e.g. „Rohrbogen 90°“ is recognized as a en 90 (an "Euro Standard”). Wrong classifications like this can be sorted out by inserting a „NO“ into the respective field in PARTproject under tabbed page General -> menu item General -> Similar to standard parts (optional) and then regenerating the catalog. Classifications have to be checked from time to time regularly.