![]() |
Sweep is the transition between two sketches on parallel planes and the same number of sketch elements.
In the part EN 10253 for example, the sweep function is used.
In the following you can see an excerpt in PARTdesigner, which exemplifies the usage.
Create a circle in a base sketch.
Create a parallel reference plane with the desired distance and on it a new sketch.
On sketch 2, in the same way, create a circle again. (Here in the example it is smaller and shifted in relation to the first circle.)
Mark both sketches under History and then click on Create sweep base.
-> The dialog box History opens.
-> The sweep is displayed in the 3D view.
![]() |
Note |
---|---|
Please also regard the chapter about the combination of Sweep and Blend! See Section 7.9.3.10.1.5.6, “ Combination of Sweep and Blend”. |
|