![]() |
In this section
you can find details on the setting options of Derivation .
General: See Section 10.4.2, “General settings”.
Enter the key terms for the views to be displayed in the input field:
DW
templates are stored under $CADENAS_SETUP/layouts/2dderivation
.
You can find the template name in the section [Template] under the key "name".
[Template]
name=drawing_4_views_frame_DIN
Also see Section 5.11.3, “ 2D derivation: Create your own Combination views (*.dw) ”.
Example: Setting 2 Rows, 2 Columns:
Shortened view is a special feature for catalogs which may look bad in the 2D derivation due to their proportions. This may happen with very long cylinders, for example. The 2D derivation would then appear to look more like a line than a cylinder.
If the part has an additional shortened view, then it is used (if activated).
Also see Section 12.2.2.4, “ Alternative 2D size Optimize drawing view on paper size / ” and Section 5.11.1, “ 2D derivation: Alternative 2D size (shortened) ”.