![]() |
5.13.10.5. Classification of
cables
5.13.10.5.2. Definition of
the single cable elements in linear form
|
|
---|---|
Prev | Next |
For each of the cable elements, a Name should exist (exception whole cable).
Following
table shows the possible attributes of the whole cable [Cable] (CNSELEK|8|2|1
):
Cables are on top level and do not have a parent element.
Following
table shows the possible attributes of cable bundle (CNSELEK|8|2|3
), cable shield (CNSELEK|8|2|4
) and
cable twist (CNSELEK|8|2|5
):
Following
table shows the possible attributes of cable cores (CNSELEK|8|2|2
):
Note: Cores are the lowest element within the recursive depiction of cables, which means they do not have child elements.
For cores the Name is build by the value of the color code of the insulation according to DIN 47100 and the diameter, which have to be set mandatorily. This allows maximal portability of cable data.
This attribute list can be flexibly enhanced if needed (preferably for the whole cable or cores). An example would be the inductivity of cable per meter (MicroHenry/m), etc.