Insert text:
Click on the button and then on the desired insertion point.
-> The dialog box Change parameter is opened and the snap appears at the selected position.
Under Text, enter the desired text and determine the appearance with the following setting options:
Font height
Angle
Text position
The red point at the "A" shows the relation to the text.
Text justification: left, center, right
Position X
Position Y
Confirm with OK.
Insert BMG Layer
Precondition is an up-to-date CNS classification. The feature is officially provided with V11 SP6.
Classify element:
Click on the element to be classified and then on the button.
-> The dialog box Change parameter is opened.
Under Group and Classification, select the desired option.
Hide classified elements.:
Click on the button.
-> The dialog area Hide classified elements. is opened.
Activate/deactivate the checkbox at desired groups or layers.
An example on this can be found under Section 5.11.2.6, “BMG Layer (DIN4003) ”.