![]() |
In order to call embedded documents in the PDF there are two possibilities:
Via click on a pin icon (see Section 10.4.12, “ Embed ”)
Via link in the characteristic attribute table (description in the following)
Precondition: The required files should be stored in the catalog (in simplest case in respective project directory). Paths have to stated relatively to path of project file.[111]