![]() |
In order to check
the integrity of a part click on the button Test part . Integrity has to be ensured to avoid error messages
in QA check and finally a faultless export to the
different CAD systems is ensured.
If there are problems when executing the function this is immediately documented in the 3D view.
In the following you can see some examples for construction errors:
A definition for "non-manifold" related to praxis is: You could not machine the shape out of a single block.
In the
3D History the affected element is marked
by a red
cross .
The dialog box Notifications shows the error.
In the dialog box QA check the error message Non manifold is also displayed.
Error message "The result is more than one solid"
The shape cannot be machined out of a single block.
In the
3D History a red cross
is displayed at affected elements.
The dialog box Notifications shows an error. "The objects are not connected".
In the dialog box QA check The error message "The objects are not connected" is also displayed".