powered by CADENAS

Manual

Manual

6.10.2.4.10. Merged projects with fixed values

The tables of the projects din_15413_a.prj and din_15413_b.prj have been merged in one project din_15413.prj.

In order to create the mapping proceed as follows:

  1. Initial situation: Select the first project to be merged. In the dialog the target project's table is missing.

  2. With a click on Add target project, add the new merged project.

  3. Repeat the procedure for the second project.

    -> Once selecting a row in the left table, on the right, the correct target project is shown.

  4. Verify the assignments by clicking on Verify all mappings .