Before projects are transferred to the directory tree of PARTdataManager or get Status 5 under SVN Administration (see Section 6.5.4.2.4, “Level 4”), new entries or changes have to be checked for any errors. You can choose from a large number of test criteria.
The call is made in PARTproject under Project selection, in the context menu of projects (Test project) or directories (Test directory).
-> The dialog box Test projects in directory is opened.
When clicking the dialog box QA check is opened. There, the results of this check are summarized in a protocol. This information allows you to make the required corrections in targeted manner. Using context menu command Save protocol as... you can save the protocol.
The second column shows the row number.
Find unused files: Finds all files which are not assigned to a project. You can either allocate such files to a project or delete them.
Calculate geometry: This function builds up the attributes (table rows) of all geometries (*.3db drawing files) on a trial basis. Attributes which lead to an “impossible” structure, such as a negative value for width across flats, are logged as an error. The calculation process may take a very long time (depending on catalog size).
Determine the maximum test time in minutes.
Also see Section 3.2.18, “Classification according to CNSORDERNO / CNSTYPECODE ”.
Test standard part identifier: The standard part identifier, e.g. ’Hexagon nut DIN 1587 $ NENN.’(displayed in PARTdataManager, in the tab of the docking window of the 3D view), which you have entered in PARTdesigner (Identification data) may, under certain circumstances, be incomplete or incorrect. For example, if column values (representing an element of the standard part identifier) prompted in certain rows are not present.
Test standard part identifier for uniqueness: ...Compares all Standard names, which may occur as the result of the various attributes (rows). If a Standard name (NB) occurs more than once, it is not unique. --> You must adapt the Standard name (NB) in a way that it is always unique!
Test order number for uniqueness: The option Test order number for uniqueness also contains a test for ReverseScripts. For this the option Test value ranges has to be activated in addition. See above.
Also see Section 3.2.18, “Classification according to CNSORDERNO / CNSTYPECODE ”.
Test short name: During the export of parts from PARTsolutions to different CAD systems, it is normal for the Standard name (NB) to be adopted as part name. As certain CAD systems have a string limit for the part name, alternatively the Short name is applied.
The Short name is a "reduced" (preferably as short as possible) version of theStandard Name (NB), limited to the - maximum length (max. 16 characters according to CAD!).
If the string of a Short name is larger than this limit, an entry is created in the log file.
Create metafiles: Creates a file in PARTsolutions export format *.ps3. This file can be imported in the relevant CAD system using the corresponding menu command of the PARTsolutions interface. The Destination directory field (file location of the ps3 file) can be activated by checking the Create metafiles option.
Maximum time for one row: ..., that should be permitted for the buildup of a single *.3db part geometry (per model). A limit of 5 minutes is recommended. If the limit is exceeded an entry in the log file follows. Check the relevant geometries and if so, make the necessary corrections in their creation.
By clicking the selected test criteria will be used and the test run will be started.
![]() |
Note |
---|---|
The test run for extensive directories may take several hours under certain circumstances. It is advisable to run the test either overnight or on a separate computer. |
Once the test run is finished, the dialog box QA check is displayed. Correct the shown warnings and errors.