Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following explains the basic instructions for use:
Activate button with simple mouse-click.
--> The buttons' function is "hanging"
on to the cursor and the button is marked by a frame.
Move the cursor to the desired location in the sketch.
--> Depending on the selected command, the object snap (circular symbol) becomes visible.
Carry out the function of the buttons through simple mouse-clicks at the desired spot (e.g. Insert line).
Automatic object snap for activated commands : If you move the cursor in the immediate area of an end, middle or intersection point, these points will be surrounded by a small circle and thus identified as a construction help point.
To improve the overview, the individual function buttons are summarized in groups with similar functions. You can also move a button group.
Right-click into a toolbar and set or remove the checkmark at the desired toolbar.
You can call the single functions in the Sketcher via shortcuts.
Advantage: Saving of time. Shortcuts will help you execute commands much quicker as with mouse.
Disadvantage: You have to remember shortcuts. Tool also show the shortcut beside the command name, so that you will learn them with time.
The following figure gives an overview on all shortcuts.
There are different modes to call them:
Under PARTdesigner -> Extras menu -> Settings... -> Sketcher (feat.) -> Shortcuts you can adjust already existing shortcuts.
In order to find the correct command be oriented towards Fig. „Overview Shortcuts “. When knowing the shortcut you can search for it in the column Key. Enter the new desired shortcut here and make sure that there is no conflict to another already existing, because the command won't work then.