Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The Remote Translation Service serves to process CAD data of a GeoSearch in the CAD in the same way as parts from a PLMsynchro catalog. Therefor, CAD live data used for the GeoSearch have to be enriched with a fingerprint by Capvidia. The same happens during a PLMsynchro run. The Capvidia license is stored on a server which can be accessed by the PLMsynchro run, but not by the CAD-Client during the GeoSearch. When the STEP file is coming from the CAD the Transremote Service is attached to create the fingerprint by Capvidia (STL is not recommended due to missing topological features). In this way the complete GeoSearch process is optimized.
Note | |
---|---|
PSWorker and so the Capvidia client can run independently of each other. GeoSearch is processed on the client or PAPPserver, however, the GeoFingerprint of Capvidia or its ZJV is used. |
In all exes (in pappserver.exe as well), the translation server always delegates the conversion, which is defined in transremote.cfg, to psworker.exe.
So only one Capvidia computer is needed, and all processes (also pappserver) apply to this, if needed.
CAPVIDIA is required in order to enrich the step files (STEP->ZJV).
This enrichment always happens on the respective client (seamless or pdatamgr or appserver in the case of WEBAPI search).
The actual GeoSearch only uses fingerprints located in the received ZJV. Then these fingerprints are transferred to the PAPPserver for searching.