powered by CADENAS

Manual

Manual

3.1.1.3. Import PARTsolutions catalog

A PARTsolutions catalog has to be initially imported in PARTdataCenter.

  1. In the context menu of Catalogs, click on the menu item Import catalog -> Import from PARTsolutions.

  2. -> The dialog box Create Catalog from PSOL is opened.

    Select your desired catalog.

    Confirm with Continue.

  3. -> The setting options PARTsolutions Import Settings are opened.

    Activate Import only existent documents in addition.

    Option Import Link Database fields: If the option is enabled then the LinkDB columns are overtaken in addition and thus are available as class features.

  4. -> The PARTsolutions catalog is imported now. After finished import you will get the respective confirmation message.

    -> The standard user interface opens again. Under menu item Catalogs, you can see the imported catalog now.

    [Note] Note

    The catalog is imported but not yet committed. You can recognize this by the blue plus signs.

  5. Initial upload

    The blue plus signs signalize that the catalog has not yet been committed.

    The blue plus signs signalize that the catalog has not yet been committed.

    Commit local Data/Catalog to Datacenter Server

    Commit local Data/Catalog to Datacenter Server

    Once the process has finished "finished" is displayed in the log.

    Once the process has finished "finished" is displayed in the log.

    Now the catalog shows green checkmarks everywhere.

    Now the catalog shows green checkmarks everywhere.