Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If you want to add one (or more) datasets to a class, do the following:
Click on Add datasets in the toolbar or in the context menu.
--> The same-named dialog opens. Check under Name, Description and Path, whether the selection is correct.
--> A dataset with timestamp ERP_PDM_NUMBER and attributes is shown.
A timestamp number is automatically created for the ERP_PDM_NUMBER. You can either take this number over or change it.
The fields Feature value of all displayed attributes can also be edited.
-> The applied datasets are shown in the PARTdataManager.
As long as you have not yet confirmed with Ok you can delete added datasets again here in this dialog.
Note | |
---|---|
After clicking Ok the datasets must be removed via Delete dataset . See Section 1.2.7, “ Delete datasets ” for more information. |
Mark the ERP_PDM_NUMBER to delete and click on .