powered by CADENAS

Manual

Manual

1.2.10.  Copy dataset

When using the command Copy dataset you can transfer values from one dataset (project line) to another dataset (project line). In order to insert the data, in the dialog box Edit dataset, use the button .

The following example shows how to use the function:

  1. In the table, select a dataset (a project line), whose values you want to copy.

  2. in the ClassificationToolbar, click on the button Copy dataset .

    [Note] Note

    The table values are copied into the clipboard. No dialog or message appears.

  3. In the table, select that line where you want to paste the copied values.

  4. In the ClassificationToolbar, click on the button Edit dataset .

    -> The dialog box Edit dataset opens.

  5. Now you can manually edit single values.

    However, you can also directly paste the copied values from the clipboard.

    Therefor click on the button . You can paste only the Table data, only the ERP data or both data types.

    In the example in hand only ERP data is inserted.

    Table data inserted from other dataset, ERP data left

    Table data inserted from other dataset, ERP data left

    Result: Now the table data are identical at matnr4 and matnr18, but the material differs.