Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
To setup the Remote Translation Service the following steps are required:
Precondition is availability of following licenses:
Adjust partsol.cfg as the following figure shows.
STEP is the preferred format, because only this can be fully analyzed by Capvidia, because the STEP format contains all topological information. STL does not contain this information.
$CADENAS_USER/psolopt.cfg
or
$CADENAS_DEFAULTUSER/psolopt.cfg
The described workflow requires the following setting: In block [CadAssistant] the key UseStepFormat has to be set on YES.
$CADENAS_SETUP/transremote.cfg
Adjust transremote.cfg as the following figure shows.
Install PARTapplicationServer (PAPPSERVER) via command line.
$CADENAS\bin\x86\64\pappserver.exe –install
Start PARTapplicationServer (PAPPSERVER) via command line.
$CADENAS\bin\x86\64\pappserver.exe –start
In pappclient.cfg, add the respective IP address.
In order for the remote conversion to be processed, the PSWorker is required.
Install psworker service via command line.
Pfad..\bin\x86\64\psworker.exe –install
For testing purposes start psworker GUI via command line. (Alternatively in the Service window of Windows)
Here you can see whether a job is processed when starting a GeoSearch in the CAD.
Pfad..\bin\x86\64\psworker.exe –gui
Open psworker config via command line and adjust the settings as shown in the following figures.
Pfad..\bin\x86\64\psworker.exe –config
In order for Capvidia to be used a CAPVIDIA Queue is needed which can be added via Plus. Finally the term CAPVIDIA has to be entered behind the Queue.
Start PARTsolutionsWorker via command line or TaskManager-Services
Pfad..\bin\x86\64\psworker.exe –start
PARTapplicationserver and PARTsolutionsWorker should be running now. (A PAPPserver has to be running in search mode at least, because it is responsible for the communication.)