powered by CADENAS

Manual

Manual

3.1.19.2.7.  Window

  • Arrange automatically adjusts the size of the single windows (3D view, Technical details, Links, etc.), when the size of the main window is changed. If the option is deactivated, then the size of the inner windows remains and scrollbars are displayed.

    [Tip] Tip

    When the single inner windows are disarranged, then you can restore the standard positions by clicking the option Arrange automatically off and on.

  • Adjust toolbars

    • Beginner

    • Default

    • Professional

    You can set via configuration file, which menus, menu items, toolbars and buttons shall be displayed at each of the three options. On this see under tweak_menuconfig_<appname>.mfg.

  • List view of parameters

  • Table view of parameters

  • List view with large 3D view

    A detailed description on the single view settings is found under ???.