Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
3.1.2.7. PARTdataManager
– ERP/PDM extensions
3.1.2.7.9.
Status indicating bitmaps for table view
(Status light)
|
|
---|---|
Prev | Next |
Preferred parts can be tagged in many ways. Not only red-green display is possible, in fact any color or icon can be used.
Status icons can signalize an Export restriction or just have indication function.
Parts for which the status light is set to green may be exported to the CAD system. Parts for which the status light is set to red may not be exported to the CAD system.
Detailed information on how to define rules is found under Section 5.6.5.2.1, “ Tabbed page "General" ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
The standard red/green display can be enhanced, so that any amount of colors (icons) can be displayed.
In any case labeling facilitates controlled usage of parts.
A useful rule could be the following for example:
Dark green = Already used at all locations Medium green = Already used at two locations Light green = Already used at one location Yellow = Used at no location, but with ERP number Red = Not according to any default
A color could be defined which signalizes whether a part is in stock. Each rule which can be deduced from table or project information is possible!
When moving your mouse over the status icon position (if highlighted), a tooltip shows up.
The status icons are also displayed in the table list view, in the list field of each variable.
Detailed information on how to define rules is found under Section 5.6.5.2.4, “Tabbed page "Display" ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.