powered by CADENAS

Manual

Manual

2.6.10.1.  Insert

The following describes how you can import your own part from your CAD system into the User library and then export it.

  1. Open or design a part (assembly) in your CAD system.

  2. Select User library -> Insert.

    PARTsolutions  
    Insert 3D
    Seamless
    Replace
    Extras
    Execute Geometric Search
    Insert Connection
    User library Insert
    Settings  
    Info

  3. --> The Select folder dialog opens.

  4. Optionally click on Create folder, in order to create a new subfolder.

    -> The New directory dialog opens. Enter the Last name and Description and confirm with OK.

  5. Select a folder in which you want to import the part and confirm with OK.

    --> The part is only located in the My Parts library.

    [Note] Note

    During the check-in process, a geometric classification (fingerprint) is automatically executed so that the own part can also be available for the geometrical search.

    Natives part from My Parts library in the PARTdataManager

    Natives part from My Parts library in the PARTdataManager

  6. Add, if desired, the data of the part by upgrading the respective table, for example:

    • In the Select folder dialog, click on Create tab files

      or

    • after the part has been inserted into the User library call up the Create tables dialog with PARTdataManager -> Table -> Edit. Select the Table tab page.

      [Note] Note

      You can only edit the tab file with admin rights.

      [Note] Note

      When importing assemblies into the User library only the assembly's table may be edited.

      Create tables

      Create tables

      More information to this you can find under Section 3.1.3.2.4, “ Table ”.

  7. Exporting own parts from the My Parts directory into the CAD system is the same process as for standard and supplier parts.

    In the PARTsolutions menu, click on Insert 3D.