powered by CADENAS

Manual

Manual

3.1.19.1.1. Catalog Quality Seal

Apply for a Quality Seal Check.

After you have passed the check, your catalog will be awarded the gold seal or the silver seal.

The seals are displayed at catalog level on the Symbols tab; additionally also in the info panel at catalog, directory, and project level (as long as the feature for the catalog has been made available).

Example: Quality seal displayed on "Symbols" tab

Example: Quality seal displayed on "Symbols" tab

Example: Quality seal displayed in "Details" Docking window

Example: Quality seal displayed in "Details" Docking window

Criteria for the awarding of a silver seal are:

  • The catalog is hosted and managed with PARTproject QA SVN

  • The catalog has passed the current automatic QA-Checker (TestMeta)

  • The catalog has clear NN, NT, NB and SHORTNB declarations

Criteria for the awarding of a gold seal are for example:

  • The catalog contains a Configuration Assistant

  • The catalog has manually configured LOD geometries

  • The catalog supports at least 3 languages