Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Due to the meaning of file name and pool path settings these two keys have their own dedicated section.
Note | |
---|---|
With the two keys PoolPath and FileName you can set the structure of pool (flat or with subdirectories) and the creation of file name. |
Note | |
---|---|
Use the appropriate configuration file for your CAD system. It is found under PARTadmin -> Category -> PARTsolutions -> Configuration files -> $CADENAS_SETUP -> if<cad name>.cfg.
|
Note | |
---|---|
For a better understanding of the examples please absolutely read Section 2.2.1.4, “Variable values - functions ”. Basic concepts are explained under Section 2.2, “CAD encompassing information ”. Thereof you can deduce how to adjust the examples according to your needs. |
Important | |
---|---|
Are you a new customer? Then you may simply use the default settings or make adjustments if desired. When you like to reuse CAD files in PARTsolutions V9 which have been created with PARTsolutions V8.1 catalogs then you have to make sure that these parts can be found in the V8.1 pool. Basically this means that the directory hierarchy (flat pool or sub-directories) and the file name must be kept. Especially regard Section 2.2.2.3, “Reuse the V8.1 pools after migration to V9 ”. Also under Section 1.1.4.3.4, “ Migration ” important notes are found. |